Get2Know Eaton Automated Transmissions: Low Mode
1:46
In this video, you will learn how and when to use Eaton’s Low Mode for automated transmissions. Eaton's automated transmissions were designed for superior reliability, performance, and efficiency. Low mode is most commonly used while driving to maximize engine braking and minimize the use of the brake pedal. For example, if you are driving down long grades, selecting Low mode by using the shift stalk after cresting a grade, can maximize engine braking and help maintain a desired speed. This driver video will educate you on how to use Low mode as you head out on the road in your vehicle. You’ll need to select D on the shift stalk to allow the transmission to go back into Drive mode. When you’re ready to stop, apply the service brake to come to a complete stop, select neutral on the shifter and pull the parking brake.
In this video, you will learn how and when to use Eaton’s Low Mode for automated transmissions. Eaton's automated transmissions were designed for superior reliability, performance, and efficiency. Low mode is most commonly used while driving to maximize engine braking and minimize the use of the brake pedal. For example, if you are driving down long grades, selecting Low mode by using the shift stalk after cresting a grade, can maximize engine braking and help maintain a desired speed. This driver video will educate you on how to use Low mode as you head out on the road in your vehicle. You’ll need to select D on the shift stalk to allow the transmission to go back into Drive mode. When you’re ready to stop, apply the service brake to come to a complete stop, select neutral on the shifter and pull the parking brake.
Get 2 Know (automated transmissions) Similar Videos
-
Get2Know Endurant XD series: High Speed Reverse in International trucks
1:07
High speed reverse is available on the Endurant XD Pro model with up to six configurable speeds for better route time in reverse. This is a great feature on job sites that require operating in reverse for long distances.
-
Get2Know Endurant HD+XD: Secondary Configuration in Peterbilt + Kenworth trucks
1:18
The secondary configuration feature in Peterbilt and Kenworth trucks equipped with Endurant HD and XD series or PACCAR TX-12 and TX-18 series transmissions allows the driver to switch between Performance Goals to tailor transmission performance.
-
Get2Know Driver Training: Using Rock Free mode in a Peterbilt truck
2:24
Get unstuck with Rock Free mode in Peterbilt trucks! Build momentum with Endurant XD Pro transmissions and get out of ditches with ease. Learn more in our video.