How does an Eaton locking differential work
0:21
Locking differentials (generically referred to as “lockers”) can lock the axles together to provide 100% of available torque to the wheel with traction. During turns, a locking differential operates like an open differential - the wheels can rotate at different speeds. However, when traction is needed, the axles can be mechanically locked together forcing the wheels to rotate at the same speed. This is especially helpful in off-roading situations when one wheel is off the ground or on an otherwise very low traction surface. When locked, the wheel in the air doesn’t receive any torque because there is no traction and the wheel on the ground receives all the torque, allowing the vehicle to move.
Locking differentials (generically referred to as “lockers”) can lock the axles together to provide 100% of available torque to the wheel with traction. During turns, a locking differential operates like an open differential - the wheels can rotate at different speeds. However, when traction is needed, the axles can be mechanically locked together forcing the wheels to rotate at the same speed. This is especially helpful in off-roading situations when one wheel is off the ground or on an otherwise very low traction surface. When locked, the wheel in the air doesn’t receive any torque because there is no traction and the wheel on the ground receives all the torque, allowing the vehicle to move.
Vehicle Similar Videos
-
EV Technology Solutions
0:30
Eaton is helping to drive adoption and evolve EV technology with our innovative power electronics, ePowertrain and power distribution and protection solutions for the EV ecosystem.
-
Eaton EV Transmission Highlights
0:43
Learn product highlights about Eaton's portfolio of efficient transmissions for electric commercial vehicles.
-
Find your traction solution - Eaton Detroit Truetrac limited slip differential
0:15
Truetrac FB-Digital-Throttle-Video-Aug-2022