How does an Eaton locking differential work
0:21
Locking differentials (generically referred to as “lockers”) can lock the axles together to provide 100% of available torque to the wheel with traction. During turns, a locking differential operates like an open differential - the wheels can rotate at different speeds. However, when traction is needed, the axles can be mechanically locked together forcing the wheels to rotate at the same speed. This is especially helpful in off-roading situations when one wheel is off the ground or on an otherwise very low traction surface. When locked, the wheel in the air doesn’t receive any torque because there is no traction and the wheel on the ground receives all the torque, allowing the vehicle to move.
Locking differentials (generically referred to as “lockers”) can lock the axles together to provide 100% of available torque to the wheel with traction. During turns, a locking differential operates like an open differential - the wheels can rotate at different speeds. However, when traction is needed, the axles can be mechanically locked together forcing the wheels to rotate at the same speed. This is especially helpful in off-roading situations when one wheel is off the ground or on an otherwise very low traction surface. When locked, the wheel in the air doesn’t receive any torque because there is no traction and the wheel on the ground receives all the torque, allowing the vehicle to move.
Vehicle Similar Videos
-
iQ-Cruise is the first AI-powered, intelligent cruise control that provides significant fuel savings.
1:01
Unlike existing standalone adaptive or predictive cruise control systems, iQ-Cruise seamlessly integrates both functions into a unified system. Thi
-
Wireless mobile machine control portfolio overview
2:46
Learn the technical highlights about our wireless mobile product portfolio, and watch our controls in action with some example operations.
-
Efficient, safe and flexible EV solutions
1:00
Learn how we are powering the electric revolution with our efficient, safe and flexible EV solutions for the distribution and conversion of power in electric vehicles.