10 in 10: Overcoming the challenges of a circular economy
13:32
The circular economy model has evolved quite significantly in the last 5 years, but the reality is a bit more challenging and the speed at which our economy is evolving isn’t moving fast enough.
Overview
 
      10 in 10: Overcoming the challenges of a circular economy
          
        
      The circular economy model has evolved quite significantly in the last 5 years, but the reality is a bit more challenging and the speed at which our economy is evolving isn’t moving fast enough.