Strengthening the weakest SCCR
4:31
A particularly important parameter for a control panel in North America is the Short Circuit Current Rating, or SCCR, which must be specified on the rating plate of the control panel according to NEC 2017. Learn more in our video.
A particularly important parameter for a control panel in North America is the Short Circuit Current Rating, or SCCR, which must be specified on the rating plate of the control panel according to NEC 2017. Learn more in our video.
Related videos for "sccr"
-
Eaton SCCR Informatiefilm
1:02
Eaton SCCR Informatiefilm
-
Bussmann series - How to operate the Bussmann series Low Profile Compact Circuit Protector
1:20
A demonstration on operating the low profile Compact Circuit Protector fused UL 98 Listed Class CC and G disconnect switch that's available in 1-, 2- and 3-poles. There is also a UL 508 Listed version for UL supplemental and IEC 10x38 fuses.
-
アーク放電とSCCRの関係
56:30
The discussion highlights that equipment with higher SCCR ratings can mitigate arc flash hazards by enduring larger faults.