S1. E2. Ask the Experts - PLCs, Part 2
31:05
In the second installment of Ask the Expert: Programmable Logic Controllers (PLCs), application engineer Travis and our Automation product manager Adam cover questions that were not answered in the first session and takes additional questions from the audience. Our experts answered the following questions: 1:30 What do I need to create a PID control loop in my process? 3:41 How can I control a variable frequency drive with a PLC? 5:02 How are PLCs used in correlation with safety applications? 7:32 Why is the data logging feature so commonly used with a nano PLC? 9:08 What is a SCADA system? 9:54 Are you planning to make any major ECS soft code assist software updates soon? 10:45 What is the best, most cost-effective way to start thinking about and learning how to program Eaton's PLCs? 12:08 What kind of sensors work with PLCs? 14:04 How redundant is the PLC and what about using Highway Addressable Remote Transducer (HART) protocol? 16:28 What kind of upfront checklist would you have that you would recommend using if you were going to build an infrastructure that uses a PLC? 20:48 How do you take PLC programming to a level beyond Ladder Logic? 26:24 Describe the API functionality of the easyE4. For more information visit https://www.eaton.com/plc
In the second installment of Ask the Expert: Programmable Logic Controllers (PLCs), application engineer Travis and our Automation product manager Adam cover questions that were not answered in the first session and takes additional questions from the audience. Our experts answered the following questions: 1:30 What do I need to create a PID control loop in my process? 3:41 How can I control a variable frequency drive with a PLC? 5:02 How are PLCs used in correlation with safety applications? 7:32 Why is the data logging feature so commonly used with a nano PLC? 9:08 What is a SCADA system? 9:54 Are you planning to make any major ECS soft code assist software updates soon? 10:45 What is the best, most cost-effective way to start thinking about and learning how to program Eaton's PLCs? 12:08 What kind of sensors work with PLCs? 14:04 How redundant is the PLC and what about using Highway Addressable Remote Transducer (HART) protocol? 16:28 What kind of upfront checklist would you have that you would recommend using if you were going to build an infrastructure that uses a PLC? 20:48 How do you take PLC programming to a level beyond Ladder Logic? 26:24 Describe the API functionality of the easyE4. For more information visit https://www.eaton.com/plc
Related videos for "9"
-
IBEW interview and PSEC tour - What works for me
49:04
Director of Eaton's Power Systems Experience Centers, Dan Carnovale, is interviewed by Laticia López of the International Brotherhood of Electrical Workers (IBEW). This is part of the IBEW's "What works for me" series.
-
Crouse Hinds IHBE LED 2020-9-29 ready
1:46
Crouse Hinds IHBE LED 2020-9-29 ready
-
Why choose the Eaton 9PX split-phase double-conversion UPS
2:19
Learn about the Eaton 9 series single-phase double-conversion UPS lines. In this video, we will focus specifically on the 9PX split-phase double-conversion UPS.