S1. E2. Ask the Experts - PLCs, Part 2
31:05
In the second installment of Ask the Expert: Programmable Logic Controllers (PLCs), application engineer Travis and our Automation product manager Adam cover questions that were not answered in the first session and takes additional questions from the audience. Our experts answered the following questions: 1:30 What do I need to create a PID control loop in my process? 3:41 How can I control a variable frequency drive with a PLC? 5:02 How are PLCs used in correlation with safety applications? 7:32 Why is the data logging feature so commonly used with a nano PLC? 9:08 What is a SCADA system? 9:54 Are you planning to make any major ECS soft code assist software updates soon? 10:45 What is the best, most cost-effective way to start thinking about and learning how to program Eaton's PLCs? 12:08 What kind of sensors work with PLCs? 14:04 How redundant is the PLC and what about using Highway Addressable Remote Transducer (HART) protocol? 16:28 What kind of upfront checklist would you have that you would recommend using if you were going to build an infrastructure that uses a PLC? 20:48 How do you take PLC programming to a level beyond Ladder Logic? 26:24 Describe the API functionality of the easyE4. For more information visit https://www.eaton.com/plc
In the second installment of Ask the Expert: Programmable Logic Controllers (PLCs), application engineer Travis and our Automation product manager Adam cover questions that were not answered in the first session and takes additional questions from the audience. Our experts answered the following questions: 1:30 What do I need to create a PID control loop in my process? 3:41 How can I control a variable frequency drive with a PLC? 5:02 How are PLCs used in correlation with safety applications? 7:32 Why is the data logging feature so commonly used with a nano PLC? 9:08 What is a SCADA system? 9:54 Are you planning to make any major ECS soft code assist software updates soon? 10:45 What is the best, most cost-effective way to start thinking about and learning how to program Eaton's PLCs? 12:08 What kind of sensors work with PLCs? 14:04 How redundant is the PLC and what about using Highway Addressable Remote Transducer (HART) protocol? 16:28 What kind of upfront checklist would you have that you would recommend using if you were going to build an infrastructure that uses a PLC? 20:48 How do you take PLC programming to a level beyond Ladder Logic? 26:24 Describe the API functionality of the easyE4. For more information visit https://www.eaton.com/plc
Related videos for "SCADA systems."
-
Reclosers
9:30
See how a recloser works on a utility power system at Eaton's Power Systems Experience Center (PSEC) during temporary and permanent faults. Topics include SCADA feeder automation systems and electronic, hydraulic, single and three phase reclosers.
-
Configuring communications for an in-line system
8:38
This video demonstrates how to set up a master protocol instance from an Eaton Feeder Automation software template to get data from the devices. The setting up of the slave protocol instance to pass data to the SCADA system is covered.