CGLine+ Web compact controller - How to replace a CGLine+ safety luminaire using the local display ?
2:30
This video is a quick maintenance guide to replace a self-contained luminaire on a CGLine+ installation managed by the CGLine+ Web Compact Controller without any device, only the local display. Installers and technicians just need to follow this step by step video. The CGline+ Web compact controller is dedicated to optimizing the monitoring and maintenance of small and medium Emergency Lighting installations. Advanced control features, such as block, rest and switch-off modes, result in a more energy and cost efficient system, with a longer lifetime. Maintenance effort and operational expenses are reduced.
This video is a quick maintenance guide to replace a self-contained luminaire on a CGLine+ installation managed by the CGLine+ Web Compact Controller without any device, only the local display. Installers and technicians just need to follow this step by step video. The CGline+ Web compact controller is dedicated to optimizing the monitoring and maintenance of small and medium Emergency Lighting installations. Advanced control features, such as block, rest and switch-off modes, result in a more energy and cost efficient system, with a longer lifetime. Maintenance effort and operational expenses are reduced.
Related videos for "web controller"
-
Ethernet connection between easyE4 and PC – via “Static IP” (Tutorial)
4:33
In this tutorial you will learn how to establish an Ethernet connection between PC and the Eaton easyE4 control relay in "Static IP" mode.
-
Programming of a user function block (UF) (Tutorial)
4:40
In this tutorial you will learn how to program a user function block (UF) for the easyE4 control relay from Eaton and how to call it in the main program.
-
CGLine+ Web Compact Controller - Comment remplacer un bloc CGLine+ via l'écran
2:30
Découvrez la facilité de remplacement d'un bloc sur une installation CGLine+ sans ordinateur via l'écran du CGLine+ Web Compact Controller