IR window FAQs
22:42
Business Development Manager for IRISS Inc. answers frequently asked questions about infrared windows for power equipment. Thank you for watching one of our many educational videos on the topic of power systems. Schedule a visit to one of Eaton's Power Systems Experience Centers in either Pittsburgh or Houston to learn more! To learn more about Eaton products and our Power Systems Experience Centers: http://eaton.com/experience To view more educational videos from Eaton's Power Systems Experience Centers: http://videos.eaton.com/experience ___________________________________________________ infared windows, IR windows, switchgear, switchboard, accousting sensing, crystal IR window, power system infared, What is an IR window? Can I put IR windows on my switchgear? Can I put IR windows on my switchboard? 0:00 - Introduction 0:55 - Will installing / retrofitting infrared windows on my equipment invalidate my equipment UL listing? (or CSA in Canada) 2:33 - What is an NRTL? 3:24 - What is the difference between UL Recognized and UL Listed? 4:18 - Will installing / retrofitting infrared windows on my equipment degrade my IP (ingress protection) rating or NEMA rating of the enclosure? 5:57 - Can Infrared Windows be installed in Arc Resistant Switchgear? 8:05 - I want to buy an Arc Resistant infrared window? Your competitor offers one. What can you offer me? 9:55 - I need a window that is rated for 65KA. What can you offer me? 11:16 - What happens to my equipment warranty from the OEM if I install (retrofit) one of your windows into my equipment? 12:52 - If I have the infrared window cover open and an Arc Flash occurs inside the equipment, will I be protected? 15:40 - Do you make windows that are Class 1, Div 2 rated? We would like to install on a piece of equipment with that designation. 16:55 - What PPE should I be wearing when interacting with an IR window? 18:54 - We want to utilize your IR windows with an ultrasound port or ultrasound sensor. Where should we mount the window for optimal ultrasound readings? 21:06 - More details about IRISS Inc. #ir #power #safety
Business Development Manager for IRISS Inc. answers frequently asked questions about infrared windows for power equipment. Thank you for watching one of our many educational videos on the topic of power systems. Schedule a visit to one of Eaton's Power Systems Experience Centers in either Pittsburgh or Houston to learn more! To learn more about Eaton products and our Power Systems Experience Centers: http://eaton.com/experience To view more educational videos from Eaton's Power Systems Experience Centers: http://videos.eaton.com/experience ___________________________________________________ infared windows, IR windows, switchgear, switchboard, accousting sensing, crystal IR window, power system infared, What is an IR window? Can I put IR windows on my switchgear? Can I put IR windows on my switchboard? 0:00 - Introduction 0:55 - Will installing / retrofitting infrared windows on my equipment invalidate my equipment UL listing? (or CSA in Canada) 2:33 - What is an NRTL? 3:24 - What is the difference between UL Recognized and UL Listed? 4:18 - Will installing / retrofitting infrared windows on my equipment degrade my IP (ingress protection) rating or NEMA rating of the enclosure? 5:57 - Can Infrared Windows be installed in Arc Resistant Switchgear? 8:05 - I want to buy an Arc Resistant infrared window? Your competitor offers one. What can you offer me? 9:55 - I need a window that is rated for 65KA. What can you offer me? 11:16 - What happens to my equipment warranty from the OEM if I install (retrofit) one of your windows into my equipment? 12:52 - If I have the infrared window cover open and an Arc Flash occurs inside the equipment, will I be protected? 15:40 - Do you make windows that are Class 1, Div 2 rated? We would like to install on a piece of equipment with that designation. 16:55 - What PPE should I be wearing when interacting with an IR window? 18:54 - We want to utilize your IR windows with an ultrasound port or ultrasound sensor. Where should we mount the window for optimal ultrasound readings? 21:06 - More details about IRISS Inc. #ir #power #safety
Related videos for "class 2 "
-
Eaton’s digital 2-pole GFCI improves performance & compatibility; adds class-leading 12 trip codes
1:31
Built on a digital platform, Eaton’s new BR two-pole GFCI breaker improves performance and compatibility for 240 V applications. And troubleshooting is now faster and easier with a class-leading 12 LED trip codes.
-
Bussmann series - How to operate the Bussmann series Low Profile Compact Circuit Protector
1:20
A demonstration on operating the low profile Compact Circuit Protector fused UL 98 Listed Class CC and G disconnect switch that's available in 1-, 2- and 3-poles. There is also a UL 508 Listed version for UL supplemental and IEC 10x38 fuses.
-
Eaton PDI PowerHub 2
4:00
Available in sizes ranging from 375 – 1.25 MVA, PDI PowerHub 2 is a powerhouse PDU. It’s industry-leading 60” wide x 40” deep true front access cabinet makes it the smallest footprint in its class.