Intelligent Notification Controller Features and Benefits
2:51
The INC can be added to any fire system because our devices are compatibility listed with the controller independent of the fire panel. In simple terms, the Intelligent Notification Controller easily replaces the capacity of two older generation Booster Power Supplies. Plus, Wheelock’s $1B installed base can be updated or extended for retrofit using the Intelligent Notification Controller and Eluxa devices. This means existing projects have an upgrade path to the latest technology. Finally, it’s UL/ULC listed for Fire, Mass Notification, and Access Control
The INC can be added to any fire system because our devices are compatibility listed with the controller independent of the fire panel. In simple terms, the Intelligent Notification Controller easily replaces the capacity of two older generation Booster Power Supplies. Plus, Wheelock’s $1B installed base can be updated or extended for retrofit using the Intelligent Notification Controller and Eluxa devices. This means existing projects have an upgrade path to the latest technology. Finally, it’s UL/ULC listed for Fire, Mass Notification, and Access Control
Related videos for "INC"
-
TPI and Eaton Panel Discussion April 26 2022 Recording
58:10
Autism Acceptance Month Guest Speaker The Precisionists, Inc.
-
Federal Law Enforcement and Industry Experts Call for Heightened Awareness and Increased Collaboration to Combat Threat of Counterfeit Products
54:13
Experts from Eaton Corporation, Pfizer Inc., and the U.S. Department of Homeland Security (DHS) participated in a panel discussion at the National Press Club in Washington, D.C. on June 23, 2011.
-
Intelligent Notification Controller (INC) Technical Video
19:50
Introduction to Eaton's INC, including features & benefits, unique system attributes, how the system works - Class A & B operation