国家電気工事規定(NEC)に基づくモーター保護:モーター回路_module 2
3:10
The video discusses how the United States and Canada use their own standards for electrical motor protection, such as the National Electrical Code (NEC) in the US, instead of the International Electrotechnical Commission (IEC) standards used in many other countries. NEC Article 430 outlines the requirements for motor circuits, including a main disconnect, short-circuit protection, motor controller, and overload protection. These components can be separate devices or integrated into one, such as the combination motor controllers classified from Type A to Type F in UL 508. Eaton's Moto starter MSC, for example, is an all-in-one device that combines these functions, ensuring compliance with safety standards.
The video discusses how the United States and Canada use their own standards for electrical motor protection, such as the National Electrical Code (NEC) in the US, instead of the International Electrotechnical Commission (IEC) standards used in many other countries. NEC Article 430 outlines the requirements for motor circuits, including a main disconnect, short-circuit protection, motor controller, and overload protection. These components can be separate devices or integrated into one, such as the combination motor controllers classified from Type A to Type F in UL 508. Eaton's Moto starter MSC, for example, is an all-in-one device that combines these functions, ensuring compliance with safety standards.
Related videos for "electric motor starters"
-
Reduced voltage soft starters (RVSS) explained | Eaton PSEC
8:51
A reduced voltage soft starter, or RVSS, is an electronic device used to start and control the speed of electric motors. RVSSs are designed to protect motors from sudden influxes in power by limiting inrush current associated with motor startup.
-
AT Systems future-proofs the electrical installation of a sewage treatment plant with Eaton products
4:54
AT system set up a modern, cost-effective power supply and control system for a new municipal wastewater treatment plant. The future-proof and energy-efficient electrical installation which can be remotely monitored.
-
Manual Motor Controllers and Motor Starters
3:40
An example of the differences between North America and IEC is article 430 of the NEC, according to which a motor circuit must fulfil at least four functions. View our video and learn more.