国家電気工事規定(NEC)に基づくモーター保護:モーター回路_module 2
3:10
The video discusses how the United States and Canada use their own standards for electrical motor protection, such as the National Electrical Code (NEC) in the US, instead of the International Electrotechnical Commission (IEC) standards used in many other countries. NEC Article 430 outlines the requirements for motor circuits, including a main disconnect, short-circuit protection, motor controller, and overload protection. These components can be separate devices or integrated into one, such as the combination motor controllers classified from Type A to Type F in UL 508. Eaton's Moto starter MSC, for example, is an all-in-one device that combines these functions, ensuring compliance with safety standards.
The video discusses how the United States and Canada use their own standards for electrical motor protection, such as the National Electrical Code (NEC) in the US, instead of the International Electrotechnical Commission (IEC) standards used in many other countries. NEC Article 430 outlines the requirements for motor circuits, including a main disconnect, short-circuit protection, motor controller, and overload protection. These components can be separate devices or integrated into one, such as the combination motor controllers classified from Type A to Type F in UL 508. Eaton's Moto starter MSC, for example, is an all-in-one device that combines these functions, ensuring compliance with safety standards.
Related videos for "main components of"
-
PDI PowerPak 2 PDU
4:27
With hundreds of possible distribution configurations, the PDI® PowerPak™ 2 PDU is the smallest power distribution unit with true front accessibility in today’s market. A patent-pending 3D access window allows true front access (TFA) for service and
-
What are the types of main breakers and their applications in residential segment? Eaton explains
0:56
Navigating main circuit breakers: A guide to protection and application
-
Low-voltage switchgear
19:28
Low-voltage switchgear has a vital role within power distribution systems. Erik Hurd, Senior PSEC Engineer, discusses what low-voltage switchgear is, design options, main features, and safety technologies.