The 10 in 10 podcast: Overcoming the challenges of a circular economy

13:32

The circular economy model has evolved quite significantly in the last 5 years, but the reality is a bit more challenging and the speed at which our economy is evolving isn’t moving fast enough. Today we will be speaking with Jean Miyeli, EMEA segment & sustainability strategy director, and Delphine Clement, energy transition sales direction, about how can we unlock these challenges and ultimately, shift our mindsets from an economic model that is linear to one that is infinite and circular. Explore all podcast episodes at: Eaton.com/10in10podcast

Featured Videos
The 10 in 10 podcast: Overcoming the challenges of a circular economy

The circular economy model has evolved quite significantly in the last 5 years, but the reality is a bit more challenging and the speed at which our economy is evolving isn’t moving fast enough. Today we will be speaking with Jean Miyeli, EMEA segment & sustainability strategy director, and Delphine Clement, energy transition sales direction, about how can we unlock these challenges and ultimately, shift our mindsets from an economic model that is linear to one that is infinite and circular. Explore all podcast episodes at: Eaton.com/10in10podcast