PXR-RCAM installation into the digital NZM
9:13
The new video explains how to install the PXR-RCAM communication module in an NZM digital circuit breaker. In addition to the necessary requirements, information about circuit breakers is given, e.g. - Overview of the circuit breakers of the NZM series - Which trip units are available - The function of the NZM-XBSM interface module in the circuit breaker.
Featured Videos
PXR-RCAM installation into the digital NZM
The new video explains how to install the PXR-RCAM communication module in an NZM digital circuit breaker. In addition to the necessary requirements, information about circuit breakers is given, e.g. - Overview of the circuit breakers of the NZM series - Which trip units are available - The function of the NZM-XBSM interface module in the circuit breaker.