70 - What is the difference between IEEE 519 of 2022 vs previous standard?
2:56
• IEEE 519 Standard Updates: We discuss the major revisions of the IEEE 519 standard, highlighting the 2022 update's focus on distributed energy resources (DERs) and the adjustments in voltage distortion limits from 5% to 8% in the 2014 update. • Application of IEEE 519 Standard: We clarified the application of the IEEE 519 standard in scenarios involving DERs. If the DERs are less than 10% of the annual average load, the standard applies as usual. However, if it exceeds 10%, additional standards like IEEE 1547 or IEEE 2800 must be considered. • Evolution of IEEE 519 Standard Documentation: We highlight the significant reduction in the length of the IEEE 519 standard documentation from about 100 pages in 1992 to approximately 20 pages in both 2014 and 2022. This change indicates an effort to make the standards more concise and focused, facilitating easier understanding and implementation. Eaton’s Harmonic Frequently Asked Question’s FAQs collection of videos hosted by Dan Carnovale can help individuals from all different levels of education understand what harmonics are and explain many different solutions for mitigating harmonics on an electrical power system. Dan Carnovale P.E. has decades of experience in power quality and harmonics and is a recognized electrical industry expert in power quality and power systems. He is the creator and director of Eaton’s Power Systems Experience Centers (PSEC) in Pittsburgh PA and Houston TX. The PSECs provide visitors live demonstrations of hands-on power quality and harmonic situations and solutions can be seen first-hand in the Power Quality Lab. Visit Eaton’s harmonics knowledge website featuring harmonic solutions, harmonic calculators, access to white papers, and more: https://www.eaton.com/harmonics See our entire harmonics FAQs playlists: https://www.youtube.com/watch?v=U36ywxWHIy8&list=PL8XobqCtN9Z8maXVw0kYDLjmhBO275-bE&pp=gAQBiAQB For an educational overview of harmonics in person, visit one of Eaton’s Power Systems Experience Centers: http://eaton.com/experience #harmonics #powerquality #electricalengineering #electricalsafety #eatonexperience #experiencecenter
• IEEE 519 Standard Updates: We discuss the major revisions of the IEEE 519 standard, highlighting the 2022 update's focus on distributed energy resources (DERs) and the adjustments in voltage distortion limits from 5% to 8% in the 2014 update. • Application of IEEE 519 Standard: We clarified the application of the IEEE 519 standard in scenarios involving DERs. If the DERs are less than 10% of the annual average load, the standard applies as usual. However, if it exceeds 10%, additional standards like IEEE 1547 or IEEE 2800 must be considered. • Evolution of IEEE 519 Standard Documentation: We highlight the significant reduction in the length of the IEEE 519 standard documentation from about 100 pages in 1992 to approximately 20 pages in both 2014 and 2022. This change indicates an effort to make the standards more concise and focused, facilitating easier understanding and implementation. Eaton’s Harmonic Frequently Asked Question’s FAQs collection of videos hosted by Dan Carnovale can help individuals from all different levels of education understand what harmonics are and explain many different solutions for mitigating harmonics on an electrical power system. Dan Carnovale P.E. has decades of experience in power quality and harmonics and is a recognized electrical industry expert in power quality and power systems. He is the creator and director of Eaton’s Power Systems Experience Centers (PSEC) in Pittsburgh PA and Houston TX. The PSECs provide visitors live demonstrations of hands-on power quality and harmonic situations and solutions can be seen first-hand in the Power Quality Lab. Visit Eaton’s harmonics knowledge website featuring harmonic solutions, harmonic calculators, access to white papers, and more: https://www.eaton.com/harmonics See our entire harmonics FAQs playlists: https://www.youtube.com/watch?v=U36ywxWHIy8&list=PL8XobqCtN9Z8maXVw0kYDLjmhBO275-bE&pp=gAQBiAQB For an educational overview of harmonics in person, visit one of Eaton’s Power Systems Experience Centers: http://eaton.com/experience #harmonics #powerquality #electricalengineering #electricalsafety #eatonexperience #experiencecenter