Short-Circuit WCRs
2:40
The Short-Circuit WCR is the UL 1008 test for a transfer switch’s ability to close into and withstand a fault current. These are the ratings which will actually appear on the UL label of the product.
The Short-Circuit WCR is the UL 1008 test for a transfer switch’s ability to close into and withstand a fault current. These are the ratings which will actually appear on the UL label of the product.
Electrical - 100 latest videos Similar Videos
-
Volts, amps, and watts in a power system | Eaton PSEC
9:08
Learn the concepts that explain the flow of electricity: volts, amps, and watts. We then explain how these fundamental units of electricity are applied in designing an electrical power system.
-
68 - If I apply harmonic producing loads, do capacitors amplify the harmonics produced?
1:59
If I apply harmonic producing loads, do I have to worry about capacitors amplifying the harmonics produced?
-
Magnum circuit breakers with Power Xpert Release (PXR) | Eaton PSEC
9:37
Magnum circuit breakers with PXR trip units offer greater insights into system health, accurate testing, and enhanced communication. With the addition of Eaton's MR2 device, they also increase operator safety by mitigating arc flash exposure.