Extending transformer temperature ratings with PEAK designs
1:01:31
This session reviews transformers designed to IEEE standard C57.154-2012. This recent standard was developed to acknowledge the advantages of Natural Esther Insulating Oils, such as Cargill Envirotemp FR3 fluid, and its application in new transformer designs that expand the capabilities of transformers to operate at higher temperatures. These new 75 degree C ratings, which Eaton refers to as PEAK transformers, provide for expanded ratings in smaller physical packages.
This session reviews transformers designed to IEEE standard C57.154-2012. This recent standard was developed to acknowledge the advantages of Natural Esther Insulating Oils, such as Cargill Envirotemp FR3 fluid, and its application in new transformer designs that expand the capabilities of transformers to operate at higher temperatures. These new 75 degree C ratings, which Eaton refers to as PEAK transformers, provide for expanded ratings in smaller physical packages.
Electrical - 100 latest videos Similar Videos
-
Celebrating 20 Years of Eaton's Power Systems Experience Centers – A Message from Mark Rumpel
0:50
Mark Rumpel, Vice President of Marketing Communications for Eaton's Electrical Sector in the Americas, highlights the 20th anniversary of Eaton's Power Systems Experience Centers (PSEC).
-
Eaton's Power Systems Experience Centers celebrate 20 years!
0:56
Eaton’s Power Systems Experience Centers celebrate 20 years of innovation! Since 2005, these state-of-the-art facilities have advanced industry knowledge by being able to expand testing, training, and demonstrations of electrical power systems.
-
SmartRack Top-of-Rack Precision AC-SRCOOL3KTP
1:39
Available separately or bundled with a 25U or 33U rack, the top-of-rack air conditioner is a self-contained cooling system for single-rack micro data centers. https://tripplite.eaton.com/25u-server-rack-integral-12k-btu-ac-unit~SRCOOL3KTP25U.