52 – Why is voltage distortion bad? Are multiple zero crossings on voltage from harmonics a bad thing?
4:18
Why is voltage distortion bad? Are multiple zero crossings on voltage from harmonics a bad thing? Voltage distortion, which can be caused by multiple zero crossings resulting from harmonics, can lead to mis-operation of electrical equipment. While it may not always be detrimental as seen with digital clocks running fast, in critical applications like welding or PLC control, it poses real challenges. In this video learn how these effects are crucial for maintaining reliable power systems. Harmonic FAQ Series What are harmonics and where do harmonics come from? Harmonics are generated from non-linear loads that typically include power electronics such as variable frequency drives (VFD) and LED lights. Harmonic current can cause excess heating of transformers and cables, damaging electrical equipment. Harmonics can also cause voltage distortion, often resulting in the mis operation of equipment during critical applications. Monitoring and measuring harmonics are critical steps in selecting the best harmonic solution to reduce the total harmonic distortion or THD on a power system to comply with the IEEE-519 standard. Power factor correction and harmonic resonance should also be considered. Eaton’s Harmonic Frequently Asked Question’s FAQs collection of videos presented by Dan Carnovale can help individuals from varying background and experience levels understand what harmonics are and explore varying solutions for mitigating harmonics on an electrical power system. Dan Carnovale P.E. has decades of experience in power quality and harmonics and is a recognized electrical industry expert in power quality and power systems. He is the creator and director of Eaton’s Power Systems Experience Centers (PSEC) in Pittsburgh PA and Houston TX. The PSECs provide visitors with live demonstrations of hands-on power quality and harmonic situations and solutions that can be seen first-hand in the Power Quality Lab. Visit Eaton’s harmonics knowledge website featuring harmonic solutions, harmonic calculators, access to white papers, and more: https://www.eaton.com/harmonics See our entire harmonics FAQs playlists: https://www.youtube.com/watch?v=U36ywxWHIy8&list=PL8XobqCtN9Z8maXVw0kYDLjmhBO275-bE For an educational overview of harmonics in person, visit one of Eaton’s Power Systems Experience Centers: http://eaton.com/experience #harmonics #powerquality #electricalengineering #electricalsafety #eatonexperience #experiencecenter
Why is voltage distortion bad? Are multiple zero crossings on voltage from harmonics a bad thing? Voltage distortion, which can be caused by multiple zero crossings resulting from harmonics, can lead to mis-operation of electrical equipment. While it may not always be detrimental as seen with digital clocks running fast, in critical applications like welding or PLC control, it poses real challenges. In this video learn how these effects are crucial for maintaining reliable power systems. Harmonic FAQ Series What are harmonics and where do harmonics come from? Harmonics are generated from non-linear loads that typically include power electronics such as variable frequency drives (VFD) and LED lights. Harmonic current can cause excess heating of transformers and cables, damaging electrical equipment. Harmonics can also cause voltage distortion, often resulting in the mis operation of equipment during critical applications. Monitoring and measuring harmonics are critical steps in selecting the best harmonic solution to reduce the total harmonic distortion or THD on a power system to comply with the IEEE-519 standard. Power factor correction and harmonic resonance should also be considered. Eaton’s Harmonic Frequently Asked Question’s FAQs collection of videos presented by Dan Carnovale can help individuals from varying background and experience levels understand what harmonics are and explore varying solutions for mitigating harmonics on an electrical power system. Dan Carnovale P.E. has decades of experience in power quality and harmonics and is a recognized electrical industry expert in power quality and power systems. He is the creator and director of Eaton’s Power Systems Experience Centers (PSEC) in Pittsburgh PA and Houston TX. The PSECs provide visitors with live demonstrations of hands-on power quality and harmonic situations and solutions that can be seen first-hand in the Power Quality Lab. Visit Eaton’s harmonics knowledge website featuring harmonic solutions, harmonic calculators, access to white papers, and more: https://www.eaton.com/harmonics See our entire harmonics FAQs playlists: https://www.youtube.com/watch?v=U36ywxWHIy8&list=PL8XobqCtN9Z8maXVw0kYDLjmhBO275-bE For an educational overview of harmonics in person, visit one of Eaton’s Power Systems Experience Centers: http://eaton.com/experience #harmonics #powerquality #electricalengineering #electricalsafety #eatonexperience #experiencecenter
Electrical Similar Videos
-
70 - What is the difference between IEEE 519 of 2022 vs previous standard?
2:56
What are the differences between the IEEE519 harmonic standard and previous standards?
-
65 - Is the utility sending me harmonics?
3:45
Is the utility sending me harmonics?
-
62 - Do I need to specify a 200% neutral on my panelboard and transformer if I have a lot of harmonics?
2:43
Do I need to specify a 200% neutral on my panelboard and transformer if I have a lot of harmonics?