How does an Eaton locking differential work
0:21
Locking differentials (generically referred to as “lockers”) can lock the axles together to provide 100% of available torque to the wheel with traction. During turns, a locking differential operates like an open differential - the wheels can rotate at different speeds. However, when traction is needed, the axles can be mechanically locked together forcing the wheels to rotate at the same speed. This is especially helpful in off-roading situations when one wheel is off the ground or on an otherwise very low traction surface. When locked, the wheel in the air doesn’t receive any torque because there is no traction and the wheel on the ground receives all the torque, allowing the vehicle to move.
Locking differentials (generically referred to as “lockers”) can lock the axles together to provide 100% of available torque to the wheel with traction. During turns, a locking differential operates like an open differential - the wheels can rotate at different speeds. However, when traction is needed, the axles can be mechanically locked together forcing the wheels to rotate at the same speed. This is especially helpful in off-roading situations when one wheel is off the ground or on an otherwise very low traction surface. When locked, the wheel in the air doesn’t receive any torque because there is no traction and the wheel on the ground receives all the torque, allowing the vehicle to move.
Vehicle Similar Videos
-
Find your traction solution - Eaton Detroit Truetrac limited slip differential
0:15
Truetrac FB-Digital-Throttle-Video-Aug-2022
-
Eaton eMobility: Power Distribution and Protection
0:30
Eaton's electric vehicle power distribution and protection portfolio combines automotive and commercial vehicle expertise with electrical insights to offer proven technologies that reliably protect both people and EV systems.
-
Eaton Differential Install Kits
0:15
Differential Install Kits FB-Digital-Throttle-Video-Aug-2022