Eaton Get2Know International Driver Training: Low Speeds
2:53
In this ultimate guide by Eaton, watch our driver demonstrate the new stalk shifter’s low speed maneuverability features for International LT Series trucks. The stalk shifter is a revolutionary feature that allows drivers to select the neutral, drive, and low gears by rotating the stalk shifter forward or backward. Additionally, drivers can manually shift the transmission by pressing the end of the stalk shifter and moving it toward or away from the steering wheel. The stalk shifter also enables drivers to activate and adjust the engine brake by pressing the stalk shifter down to different increments. With this ultimate guide, you’ll learn everything you need to know about the stalk shifter and how it can help you navigate low speed maneuvers with ease.
In this ultimate guide by Eaton, watch our driver demonstrate the new stalk shifter’s low speed maneuverability features for International LT Series trucks. The stalk shifter is a revolutionary feature that allows drivers to select the neutral, drive, and low gears by rotating the stalk shifter forward or backward. Additionally, drivers can manually shift the transmission by pressing the end of the stalk shifter and moving it toward or away from the steering wheel. The stalk shifter also enables drivers to activate and adjust the engine brake by pressing the stalk shifter down to different increments. With this ultimate guide, you’ll learn everything you need to know about the stalk shifter and how it can help you navigate low speed maneuvers with ease.
Get 2 Know (automated transmissions) Similar Videos
-
Get2Know Endurant XD series: High Speed Reverse in International trucks
1:07
High speed reverse is available on the Endurant XD Pro model with up to six configurable speeds for better route time in reverse. This is a great feature on job sites that require operating in reverse for long distances.
-
Get2Know Endurant HD+XD series automated transmissions: Performance Goals
1:10
Because we know there is no one-size-fits-all solution for the trucking industry, the Endurant family of transmissions uses selectable Performance Goals, which combine transmission shift points and clutch calibrations with unique software.
-
Get2Know Endurant HD+XD: Secondary Configuration in Peterbilt + Kenworth trucks
1:18
The secondary configuration feature in Peterbilt and Kenworth trucks equipped with Endurant HD and XD series or PACCAR TX-12 and TX-18 series transmissions allows the driver to switch between Performance Goals to tailor transmission performance.